Industry Online Support
Technical Forum
7/23/2009 2:31 PM | |
Joined: 10/7/2005 Last visit: 9/23/2023 Posts: 2987 Rating:
|
Hello Naga firstly, you are correct, a flashing RUN LED indicates that this is theStandby CPU and that it is in cyclic operation. As for S11 and S12 I belive you mean SI1 (Serial Interface 1, this is the AS511 programming port) and SI2 (Serial Interface 2, this is the optional second interface). According to the manual BOTH LED's should be off, if they are lit it indicates an internal error. Hereare the manual links,have a look at especially chapter 4.1 of volume2/2: S5-155H Programmable Controller (CPU 948R / CPU 948RL) Volume 1/2 S5-155H Programmable Controller (CPU 948R / CPU 948RL) Volume 2/2 I hope this helps |
Cheers |
|
Follow us on