Industry Online Support
Technical Forum
10/12/2013 8:00 AM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating: (715) |
Hello, No, the S5 has no hardware config like S7. The addressing is done by slot place or Dip switches at the module, some modules need special functionblocks. The problem is that each family of CPU has it's own way off addressing, even within a family diferent CPU may have different addressing. So you have to check manuals of both CPU for the right adresses of your hardware. SIMATIC S5-S7 Migration Support - Technical DocumentsIs a good place to look for documentation on the S5 Regards, Marcjan |
Problem solved? |
|
10/31/2013 1:54 PM | |
Posts: 2 Rating: (0) |
dear dhinagaran.v No you just have to configure the CPU type at the beging and the memory amount good luck |
Follow us on