Industry Online Support
Technical Forum
7/30/2008 8:05 PM | |
Posts: 2661 Rating:
|
These LED's indicate the interface(IF1/2) status, not necessarily faults only. There could be many reasons why these LED's are lit-up. Check chapter 3.3 of section 5 in the following manual: COM 525 Programming Package for the Communication Processors CP 524 and CP525 (S5-DOS) Volume 1/2 |
Follow us on