7/29/2010 8:38 AM | |
Joined: 10/7/2005 Last visit: 12/20/2024 Posts: 3029 Rating: (1058)
|
Hello elvakof a good starting point for anyone who is new to S5-> S7 upgrades is the link below: SIMATIC S5-S7 Migration Support The technical documentation section is especially useful and the two must have manuals for you arethe specific one for your S5 CPU as a reference document (it'll have all the S5 commands and explanations for them in it) and the "from S5 to S7"manual (which will also already be in the Documentation section of your SIMATIC program grouphave Step 7 installedbut can also be downloaded from the above link). And here are also afew additional links that may be helpful: Considerations for the conversion of S5 programs to S7 What is the difference between STEP 7 and STEP 5 with regard to the operations for indirect addressing? Over and top of that you'll find more FAQ's and Forum entries via https://support.automation.siemens.comcocerning thismatter,which may come in handy as you progress with your conversion. I hope this helps and good luck |
Cheers |
|
7/30/2010 3:52 AM | |
Posts: 2 Rating: (0) |
Hi fritz Thank you for your great support. It is very useful for me. BR// elvakof |
This contribution was helpful to1 thankful Users |
Follow us on