6/20/2012 9:25 AM | |
Joined: 10/7/2005 Last visit: 6/8/2023 Posts: 2968 Rating:
|
Hello karolewsky the order number and linkfor the additional PG interface module is:6ES5752-0AA53 As it is in the cancellation phase you may need to searchthe web to find one (Siemens may also still be able to deliver one, pelase check with your local Siemens rep.). Alternatively, you may consider to use an external AS511 capablePG Multiplexer such as the ones available HERE. I hope this helps |
Cheers |
|
This contribution was helpful to
1 thankful Users |
6/21/2012 7:31 AM | |
Joined: 10/7/2005 Last visit: 6/8/2023 Posts: 2968 Rating:
|
Truth be told, I do not know for sure (and have never tried this). I can tell you though that the "main purpose" of the 752-0AA12TTY module is for usage with RK512 computer links, 3964(R) data as well as as "open driver" dara transmissions. Beinga TTY interface, it may very well also be useable as an AS511 PG interface, but I can really only speculate here. Note that it does havea 25 Pinconnector, soyou'd need to make up a customcable for your PG (see the SIMATIC S5-135U/155U System Manual for the details). I suggest you get first hand advise from Siemens concerning its useablity for your purpose via asupport request, perhaps others here may know for sure too though and will advise you. I hope this helps |
Cheers |
|
Follow us on