5/6/2012 2:06 PM | |
Joined: 12/1/2009 Last visit: 9/5/2024 Posts: 672 Rating: (147) |
Dear KG*, which S5 CPU do you have and what FB numbers is giving you the problem? Did you tried to upload the specific block seperate? Pending on the CPU you are using there are maybe some standard blocks, which are buildin the firmware of the CPU and do not requireand cannot be uploaded. Regards. |
Give us your feedback and show us your respect! |
|
5/6/2012 2:49 PM | |
Posts: 13 Rating: (0) |
Dear TIBI68, The CPU is 100U and the block is FB8. And i tried to upload the block seperately but that too did not work. There too it gives Checksum error. |
5/6/2012 2:59 PM | |
Joined: 12/1/2009 Last visit: 9/5/2024 Posts: 672 Rating: (147) |
Hello KG*, very strange,can you go online andsee the inside of the block? What is the name of the FB? Is that the only block you have trouble with? Regards. |
Give us your feedback and show us your respect! |
|
Follow us on