11/10/2016 6:57 AM | |
Joined: 8/3/2013 Last visit: 9/7/2022 Posts: 4 Rating:
|
Dear All, Here I involved in S5 to S7 conversion project. S5 - 942H to S7 412-5H System. After conversion , i found some errors follow, L 'DB'; T lok_kcpar [0]; CALL FC 14 ( SSNR := B#(0,1) , A_NR := B#(0,0) , ANZW := MW 176 , QTYP := B#(0,0) , DBNR := 0 , QANF := 0 , QLAE := MB 154 ); Errro log: E Ln 000207 Col 009: Constant format for data type INT does not fit the formal type WORD of the formal parameter DBNR. E Ln 000208 Col 025: Actual data type BYTE does not fit the formal type INT of the formal parameter QLAE W.r to manual, i came to know FB244 send block converted to FC14 but error seems like data type not matching & improper DB number assignment. I need suggestion to rectify this issue by fix this error or shall i use new blocks for communication. Regards, Mohan Kumar AttachmentReference Images.docx (75 Downloads) |
Follow us on