Industry Online Support
Technical Forum
8/22/2012 3:34 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (308) |
Hello, There is something wrong with the second order number in your question. 441 cards are outputs, no inputs. Floating or not has to do with galavnic separation (optocoupler for instance)between the internal PLC powering and the load voltage of the in/out channelsand and/or between individual channels. See the schematic representation in the manual of the S5-95U, chapter 15 (http://support.automation.siemens.com/WW/view/en/1091648) |
Best regards |
|
Follow us on