1/3/2008 10:18 PM | |
Posts: 58 Rating: (0) |
hi everybody, another problem of migration jejeje, Can you help me? AttachmentLIST_MIGRATION_CAL7.pdf (412 Downloads) |
1/3/2008 10:41 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (318)
|
Hi, There are more differences between a AI460 and the AI465, the AI450 is a better card and could have more difference between the channels. Please look to the getting started of the analog cards to make the right decision.... SM331; AI 8x12 Bit Getting Started part 1: 4 -20mA SM331;AI 8x12 Bit Getting Started Part 2: Voltage and PT100 SM331; AI 8 x 12 Bit Getting Started part 3: Thermocouples Wath I do with a conversion of S5 to S7 is starting up STEP7 and look in the hardware configurator which cards could do the job. Further you must realise that cheaper cards will do less for you and there is less filtering so that you have to look very carefully to the earthconcept... |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
1/4/2008 3:19 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (318)
|
Hi Navnag, A good tip, thank you for the extra information ! Some AI have the possibility to do the correction, the 6ES7331-7KB02 {internal compensation}/ -7KF02 {external compensation}/ -7PF11 {via reference junction}could read Thermo couple elements. See the handbook S7-300 Module datafor more information about those AI... |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on