9/25/2008 11:25 PM | |
Posts: 16 Rating: (0) |
Can you program an simatic s5 CPU with Step 7 software? Is it backwards compatable? |
9/26/2008 1:10 AM | |
Joined: 11/30/2006 Last visit: 6/7/2024 Posts: 118 Rating: (11) |
It is not possible.
|
9/26/2008 4:42 AM | |
Posts: 17 Rating: (3) |
Dear: STEP7 is not an update of Step5. They are two different lines of products. |
9/26/2008 7:13 AM | |
Posts: 487 Rating: (36) |
Hi Have a look at http://www.ibhsoftec-sps.de/german/Produktauswahl_S5_S7.htm With this software you can use a FCxx from S7 and save it to a FBxx for S5 .But obviously all of the S7 stuff cannot be used in S5 ( and viceversa) If you need to port a S7 program to S5 try this out. Bye ps .also a english part of the site http://www.ibhsoftec-sps.de/english/Selection_Software.htm Eric |
Last edited by: aikona at: 9/26/2008 7:14 AMadded english site |
|
9/26/2008 2:07 PM | |
Posts: 16 Rating: (0) |
I didn't think so. I was just curious if it was possible. Thanks for the input. |
9/26/2008 4:16 PM | |
Posts: 133 Rating: (9) |
Hi Assetmngr Sorry but S7 and S5 are two different software packages . Also the Hardware is different. S7 is not backward compatible with S5. Cheers |
Follow us on