7/21/2021 7:29 AM | |
Joined: 11/7/2019 Last visit: 12/8/2021 Posts: 11 Rating: (0) |
In the process of communication between the controller and the TIF portal 15.1, the connection was lost. When inspecting the controller, it turned out that the lamps on it did not light up, and all the connected modules did not work either. When power is applied, the diodes blink once and nothing else happens. Only the Ethernet communication lamps are blinking. There were no short circuits and other things in the network (before that the controller worked for 3 months). Physical disassembly revealed no burnt elements. The only thing you can lean on is that during the firmware process, the patch cord could move away from the connector in the computer. What could be wrong with the controller and how to fix it? Link to videofile: Video |
Last edited by: Meezelmao at: 07/21/2021 08:22:09Last edited by: Jen_Moderator at: 07/21/2021 10:25:39Embedded video. |
|