3/15/2018 2:29 AM | |
Joined: 10/7/2005 Last visit: 3/27/2025 Posts: 3043 Rating:
|
a one page overview that lists number of I/O Devices per CPU and/or CM/CP would be a great, but I am not aware of its existence. The tech spec of each CPU will give you this info though and it is for example 128 for a 1512SP F-1 PN CPU and 512/128 respectively for the two on-board Interfaces of a 1518-4 PN/DP CPU. Note though that the number of I/O devices with prioritized startup is generally lower and the same applies for number IRT I/O Devices (in case you want to use these features). In case you are planning of connecting DP Slaves to the Profinet via an IE/PB Link, be aware too that you must include each DP Slave in the Profinet I/O Device count. |
Cheers |
|
This contribution was helpful to
1 thankful Users |
Follow us on