12/28/2012 2:53 PM | |
Joined: 4/4/2006 Last visit: 7/15/2025 Posts: 7 Rating:
|
Hello, the ramp up time in the drive is p1120 and the ramp down is p1121. If you need two different ramp times as written,I propose using twodrive data sets (DDS), one for normal operation and one for jog operation. There inshall be all the same except the setpoint source, the jog commandand the ramp times. The list manual will help you, at first it looks big, but the function diagrams are self explaining. You will find it: http://support.automation.siemens.com/WW/view/en/59745599 Best regards |
1/2/2013 6:11 PM | |
Joined: 9/16/2008 Last visit: 5/7/2025 Posts: 60 Rating:
|
See this example http://support.automation.siemens.com/WW/view/en/56749384 check out page 22 in the pdf If you have a Siemens HMI- this can also be used to directly read and write drive parameters I hope this helps |
Follow us on