6/27/2023 8:12 AM | |
Joined: 12/13/2008 Last visit: 4/8/2025 Posts: 17 Rating:
|
It is possible to connect S7-1200 V2 and V3 to redundant WinCC Profeesional V17 Upd6 servers? |
6/29/2023 7:13 AM | |
Joined: 8/3/2009 Last visit: 4/17/2025 Posts: 15311 Rating:
|
Hello danailp Yes you can connect to the S71200 PLC in WInCC Professional. It does not matter if you use a single station or a redundant project. Which PLC do you use exactly? often its also a matter of communication ressources: https://support.industry.siemens.com/cs/ww/en/view/109479986 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on