Industry Online Support
Technical Forum
9/7/2009 10:50 AM | |
Joined: 1/23/2009 Last visit: 7/20/2024 Posts: 29 Rating: (10) |
Hello, I want to connect S7-1200 with step motor. I know that I have to use Axis tehnological object and PLCopen function blocks in STEP 7 Basic. Between PLC and step motors must exist modul which will convert the pulse signal to the movement of motor. (like ET 200S-Module 1 STEP; link: https://www.automation.siemens.com/simatic/regelsysteme/html_76/produkte/sb-step.htm ) Am i right? Can I provide a step motor control without this module, only with S7-1200? Thanks Gaspar |
Be creative while inventing ideas and be disciplined while implementing them... :) |
|
Follow us on