11/9/2011 11:40 AM | |
Posts: 2 Rating: (0) |
Hi guys, I'm running S7 Basic V10.5 to a 1200 CPU via profinet from PC and for some reason the clock memory bits do not pulse when I run the program. I've followed all the steps from various manuals and even downloaded a global library file (attached) where the clock and system bytes have been set up but to no avail. If anyone has made this work I would really appreciate some help...................been struggling for 2 days
AttachmentClockMemory.zip (1160 Downloads) |
11/9/2011 12:18 PM | |
Joined: 8/31/2010 Last visit: 4/29/2024 Posts: 1509 Rating: (222) |
Hello Eual, The attached global library is of v11 library format. It may not work properly in your case. Try with the attached library which is compatible with STEP 7 v10.5. For detail of that library refer here - How can you avoid overwriting the flags that are allocated for system and clock memory bits in the user program? Hope this helps. Your feedback is most welcome AttachmentS7-1200_PLC_tags_Mem_Bits.zip (1253 Downloads) |
Like it? Rate it! |
|
This contribution was helpful to1 thankful Users |
11/9/2011 12:36 PM | |
Posts: 2 Rating: (0) |
Hi Ganes10, will try it and give feedback. Tnx!
|
1/25/2013 12:09 PM | |
Posts: 1 Rating: (0) |
I had the same problem. Only what helped - FIRMWARE FLASH |