5/18/2013 4:44 PM | |
Posts: 113 Rating:
|
Have been playing with TSEND_C. Screen shots attached. When I drag TSEND_C in to my FC the system automatically creates TSEND_C[FBxxxx] and TSEND_C_DB[DBxx], both are locked. I then create a DB of type TCON_Param. The system lists these three items in System Blocks / Programme Resources. Enter the TCON_Param DB and set the ID to a unique number. You can set the values that TSEND_C will use either in the TCON_Param DB or in the Properties of the TSEND_C instruction though I sometimes had problems, I think it was when I had both the Properties and the DB open at the same time. If you make changes in the TCON_Param DB and download them, don't forget to restart the CPU or the changes won't take effect. So the answer to my own question is 'Yes' you have to create a DB of type TCON_Param. I will have a play and see if the same applies to TM_MAIL. AttachmentTSEND_C.pdf (235 Downloads) |
Follow us on