9/9/2015 9:31 AM | |
Joined: 6/12/2014 Last visit: 12/19/2024 Posts: 1 Rating:
|
Hello! I have a S7-1200 with 4.1 firmware. I am trying to communicate with it using Modbus tcp. Reading data from the PLC works fine. When I try to write, It sends back: Exception Response: Illegal Data address. The MB_server block's status changes to 8383. During my attempts I found that if my MB_HOLD_REG db has 5 elements in it, I have to write all 5 of them to be able to write. If I write 1 the error comes back. What do I need to change to be able to write only 1 element? ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 9/9/2015 3:47:44 PMNew subject after splitting |
|
Follow us on