6/7/2017 9:28 AM | |
Joined: 12/7/2009 Last visit: 3/17/2025 Posts: 33 Rating:
|
Hi, In view of Industry 4.0 revolution, of late we are facing a new requirement in which a data table need to be pushed directly into the SAP database from a S7-1200 station. SAP is currently an established enterprise software to manage business operations, the data analysis & presentation is managed by SAP server & it can have clients all around the globe. So the requirement is also seems to be very genuine that if there is a method to push the production data in almost real time into a dedicated structured table in the SAP database or an SQL database. Further integration with SQL database & SAP will be left to IT. Need to understand if this is possible to achieve from S7-1200 & if yes any sample application is available. Adding IEC or DNP3 modules to S7-1200 station is also allowed if possible. Thanks in advance. |
8/11/2017 2:14 PM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating:
|
New question published by klllll is split to a separate thread with the subject TRNASFER CSV FILE INTO SAP USING SOME .NET MODULE . Best regards |
Follow us on