1/4/2013 4:20 PM | |
Joined: 9/8/2009 Last visit: 7/17/2023 Posts: 1410 Rating:
|
1. libnodave at Soureforge.net 2. various modbus tcp/ip clients |
1/4/2013 4:22 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating:
|
Hello PC access is not for free. There are new SP available: http://support.automation.siemens.com/WW/view/en/60035301 PC access was for S7-200, but you could in theory use it with S7-1200: http://support.automation.siemens.com/WW/view/en/41928929 As you will see, there are restictions in the usage of pc access with S7-1200 because pc access was developped for S7-200. So why not using the standard Simatic Net OPC Server. Since V8.1, S7-1200 is released there. Here a link telling you how to proceed. http://support.automation.siemens.com/WW/view/en/39960679 And you can still have a VB application acting as OPC client |
Best regards |
|
This contribution was helpful to
1 thankful Users |
Follow us on