1/27/2016 11:24 AM | |
Joined: 5/12/2006 Last visit: 2/3/2023 Posts: 21220 Rating:
|
Hello, no with Step7 V5 is not possible to do a right diagnostic for the S7-1200. You should install TIA Portal for this. Depends on which PLC you have and which FW Version (i have asked for, you not answered!) you need the right version of TIA Portal. Easy way is to download the TIA TRIAL Version and diagnostic the PLC. Download is available here: https://support.industry.siemens.com/cs/ww/en/view/78793685 You only need the TIA Basic for the S7-1200. But if you haven't TIA Portal at the moment then i think you haven't programming and load the PLC, so you should contact the persion which have done this for help.
Chtristoph |
Follow us on