9/10/2015 8:48 PM | |
Posts: 3 Rating:
|
Hello Denilson Pegaia, We have a customer who has the S7-1200 CPU 1215 working as a Modbus Client they want to pull data from a device working as a Modbus Server that collect sensors data from us. The PLC is FW v4.0, and they juse TIA Portal V13, when they try to initiate the communication the STATUS parameters stores two error, 7002 and 8086 and the connection never get established. Do they need to use that parameter to establish connection? Kind regards, Armando ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 9/11/2015 9:33:52 AMNew subject after splitting |
|
9/11/2015 12:40 PM | |
Posts: 3093 Rating:
|
Hello Armando, Regards, |
Last edited by: Kaulquappe at: 9/11/2015 12:41:21 PM |
|
11/8/2017 2:52 PM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating:
|
New question published by metalknight is split to a separate thread with the subject S7-1200 CPU 1215 communication with Modbus Server - Data never transfered. Best regards |
Follow us on