9/23/2020 10:46 AM | |
Joined: 8/4/2015 Last visit: 9/11/2024 Posts: 7 Rating: (0) |
Hello All, I don't want to open new topic as this one looks similar to mine problem. I have S7-1200 CPU with SM1231 module and I want to receive analog signal from ABB ACS800 inverter. I made connection as on attached drawing and I have very big signal fluctuations and signal has some offset (e.g. instead of 250 A I have about 180 A). I need your advice how to properly make all connections on SM module to make signal clear? ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 09/25/2020 10:28:15New subject after splitting |
|
Follow us on