Industry Online Support
Technical Forum
12/9/2014 9:17 AM | |
Posts: 1 Rating: (0) |
Hello, I have a problem downloading software into a new S7-1200 DC/DC/DC PLC. The details are shown in the attached PDF-file. Even downloading an empty project with the correct hardware configuration gives 2 errors: - Internal system error (error code: 0x8000112100000089) - Please contact SIMATIC support.. - Communications error (error code -109): ServiceNotConnected The software on the notebook is working correctly (TIA Portal V13), and the used ethernet cable is fine. Downloading and monitoring the HMI panel in the network is no problem with the same equipment. What can be the cause of these errors? I searched for the error codes, but with no results. Thank you!
AttachmentPLC error.pdf (173 Downloads) |
Last edited by: Stef_VL at: 12/9/2014 9:53 AM |
|
12/9/2014 3:59 PM | |
Joined: 7/7/2010 Last visit: 4/25/2024 Posts: 14629 Rating: (2348)
|
I would do as suggested and submit a Support Requestand be sure to send your project as an archive or zip file. |
science guy |
|
4/12/2017 12:57 PM |
|
Joined: 3/13/2016 Last visit: 4/12/2024 Posts: 11 Rating: (0) |
...and wait few weeks for an answer |
Follow us on