4/11/2014 12:11 PM | |
Posts: 2 Rating:
|
ear Experts, dear Colleagues. Please help me with any advice in the next issue. I use RS232 module with S7-1212 C DCDCRly. i have dowload the program set x 25 and the library to send and receive sms version TIA 10.5 in this link https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&objId=40616248&nodeid4=20229805&load=content&lang=fr&siteid=cseus&aktprim=4&objaction=csview&extranet=standard&viewreg=WW when i upload the project in CPU S7-1200 they send me a sms for initialisation but when it receive a request msg with keyword it should sent a response to the receiver, but it don't sent a reponse, please help me, i joined a screen from the simulation on line Could you please tell me what could be the reason? I would appreciate any advice. Thank you inadvance. |
Last edited by: manel88 at: 4/16/2014 5:00 PMLast edited by: manel88 at: 4/16/2014 12:06 PMLast edited by: manel88 at: 4/11/2014 4:44 PM |
|
Follow us on