3/9/2017 2:38 PM | |
Joined: 2/15/2017 Last visit: 1/19/2023 Posts: 5 Rating:
|
Hi, here is complete configuration: CPU 1214C DC/DC/DC V4.0 FS 05 (6ES7 214-1AG40-0XB0) CB 1241 (RS485) V1.0 (6ES7 241-1CH30-1XB0) SM 1234 AI4/AQ2 V2.0 (6ES7 234-4HE32-0XB0) I did factory reset and after first startup (after firs hardware configuration and program download) everything was OK. But after power supply reset the fault came back again. There is Diagnostic buffer log in attachment with last power reset from event 11. With only HSC 2 enabled there is same issue with belonging HW_ID. I get same issue with three CPUs i have. I'll purchase TIA 14 and try. AttachmentCPU1214_DIAG.txt (343 Downloads) |
Last edited by: windberry at: 3/9/2017 2:49:05 PM |
|
3/10/2017 4:47 PM | |
Joined: 4/20/2007 Last visit: 12/15/2022 Posts: 710 Rating:
|
I guess I found an answer here :), thanks! |
Last edited by: Ton Verra at: 3/10/2017 4:48:13 PM |
|
This contribution was helpful to
1 thankful Users |
5/11/2017 4:31 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4839 Rating:
|
New question published by mdm is split to a separate thread with the subject TIA V14 sp1, CPU Error: Memory Card Error: Version of Configuration Description unknown CPU or incompatible CPU. Best regards |
3/8/2018 2:27 PM | |
Joined: 8/21/2014 Last visit: 12/20/2022 Posts: 688 Rating:
|
New question published by anil12 is split to a separate thread with the subject Help with uploading a program from s7-1200 1215dc/dc/dc with tia portal . Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on