10/14/2009 12:58 PM | |
Joined: 1/8/2007 Last visit: 9/5/2022 Posts: 18 Rating: (0) |
It's possible to make comunication between S7 1200 and Wincc Advance 2008. many thanks for your request Javier |
10/14/2009 2:58 PM | |||
Joined: 5/28/2008 Last visit: 10/23/2024 Posts: 1343 Rating: (141) |
Have you seen this? HMI simulation s7-1200 S7-1200 and HMI regards |
||
3/18/2010 4:46 PM | |
Joined: 9/23/2005 Last visit: 1/17/2025 Posts: 4394 Rating: (1463)
|
Hi, The FAQ “How do you access tags of S7-1200 with a panel or RT configured with WinCC flexible 2008 SP1?” http://support.automation.siemens.com/BR/view/en/38111886 (Intranet) shows how to communicate WinCC flexible 2008 SP1 with S7-1200. Despite of not 100% homologate, it works with some restrictions. The tip is to program a S7-300/400 connection and gives rack=0 and slot=1. |
Denilson Pegaia |
|
This contribution was helpful to1 thankful Users |
7/29/2010 11:32 PM | |
Joined: 7/7/2010 Last visit: 1/17/2025 Posts: 15541 Rating: (2465) |
Thank you! |
science guy |
|
7/30/2010 12:14 PM | |
Joined: 9/23/2005 Last visit: 1/17/2025 Posts: 4394 Rating: (1463)
|
You are wellcome :) |
Denilson Pegaia |
|
Follow us on