11/14/2018 11:44 PM | |
Joined: 10/13/2017 Last visit: 2/5/2025 Posts: 4 Rating:
|
Solved! Thanks Galen. "The CPU has not supported that option for LED since the 02 versions. The control of the Link LED was moved to the port hardware and is no longer under CPU control." Used the Profinet Library with instruction called, LPNDR_ReadGlobalInfo. Key for this was to execute the block using a clock bit, and also having it point at Profinet_1 not the individual ports. Having the DataRecord point to the array [1..2] of "LPNDR_typePortLinkState", not [0..1]. I receive a 1 when linked, and a 2 when not. See image attached. |
Last edited by: dlevine at: 11/14/2018 11:47:07 PMLast edited by: Jen_Moderator at: 11/15/2018 10:00:04 AMOptimized link. |
|
This contribution was helpful to
1 thankful Users |
Follow us on