2/25/2016 2:35 PM | |
Posts: 3 Rating:
|
HI EVERYONE PLZ HELP ME we have 11 i/p and 4 o/p. we are using s7-1214 plc and cb1241 rs485 card for mod-bus communication. we need to transfer the I/Os status to the master PLC ,our PLC is slave. in this program i builded program and created separate I/Os mems and also configured 'comm of modbus' and 'slave' block, i was assigned holding reg add 0-30 bool . now i need to transfer/ move/ assign the mem add(from-M1.2 to M2.6) to the holding reg which is further accessible on modbuss. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 2/26/2016 9:18:50 AMNew subject after splitting |
|
Follow us on