1/6/2015 2:54 PM | |
Joined: 4/24/2006 Last visit: 1/20/2025 Posts: 8808 Rating: (1173) |
Hello Aruljothi, At the moment it is not possible. So use the workaround mentioned by huggy_d1. But firmware version 4.1 and PLCSim v13 + SP1 will change it. (Then it will be possible to simulate ) See the following link: Firmware Version V4.1 released for S7-1200 CPUs Best regards, Wizard |
This contribution was helpful to5 thankful Users |
1/6/2015 7:33 PM | |
Posts: 8946 Rating: (999) |
Good to know. But anyhow, the CPU 12xx CPU is not very expensive, so you may buy one for testing and Simulation purposes. |
This contribution was helpful to1 thankful Users |
3/22/2017 11:01 AM | |
Joined: 2/6/2015 Last visit: 1/19/2025 Posts: 10 Rating: (0) |
Dear Arul, Yes it is possible. |
Follow us on