2/25/2018 8:52 AM | |
Posts: 19 Rating:
|
1. S7-1200 communicates with 5 Modbus slave(devices) via Modbus TCP / IP protocol. 2. PLC: S7-1200 As Modbus Tcp Client(Master): ---deleted Link--- 3. Modbus Slaves(Modbus Simulator): ---deleted Link--- AttachmentFC03 Read Holding Registers - Modbus Tcp Server V4.1.mbs.zip (1581 Downloads) |
Last edited by: Jen_Moderator at: 2/26/2018 9:44:51 AMDeleted Links and added file as an attachment. |
|
This contribution was helpful to
4 thankful Users |
10/1/2018 8:26 PM | |
Posts: 1 Rating:
|
Hi, Could you send me TIA project or link to this project. I need to read from 3 Modbus slaves and I am having some issues. Thank you Robert |
11/30/2021 4:58 PM | |
Joined: 6/16/2015 Last visit: 2/5/2025 Posts: 4 Rating:
|
What do I do with a .MBS file?? |
Follow us on