2/4/2014 7:53 PM | |
Joined: 1/22/2014 Last visit: 3/20/2025 Posts: 32 Rating:
|
Hello Owie and Kaulquappe, Nice to you that you replied. It is the first time that I use TC_CON/RECV/DISCON functions and therefore I use the nice Set32 that Siemens put available on their site. That example Set32 is working with steps and only one step is valid at a time. Like you see in network 5 (see annexed, I hope this upload is allowed), when the TCON block reports an error (Step 3) TDISCON is not executed because TDISCON himself has a problem… and then like you write, TCON try again to connect and make error. I was thinking that a Siemens Set 32 was ready to play, maybe it is necessary to put the general #REC input of the FB as a negative condition before the TDISCON to be sure that he will really (tried) disconnected. Thanks and best regards AttachmentSet32_SMS_Recv_FB11.pdf (203 Downloads) |
Follow us on