8/17/2010 9:37 PM | |
Joined: 10/1/2008 Last visit: 1/27/2025 Posts: 21 Rating:
|
The ability to receive variable length messages was added in firmware update V1.0.2. It is called "Ad hoc mode". http://support.automation.siemens.com/WW/view/en/38710558 PROFINET TCP "Ad hoc mode" "Ad hoc mode" for TCP is supported by the S7-1200. (The "Ad hoc mode" exists only with the TCP protocol variant.) Assign a value of "65535" to the LEN parameter to select "Ad hoc mode". With "Ad hoc mode", a maximum of 1472 bytes can be received. This affects the descriptions of the TRCV_C and TRCV instructions in Section 6.2.5 "Open Ethernet communication" of the 11/2009 version of the S7-1200 System Manual. |
This contribution was helpful to
1 thankful Users |
8/18/2010 12:25 PM | |
Posts: 5 Rating:
|
Galen many thanks for your help. |
Follow us on