2/25/2016 5:57 PM | |
Posts: 2 Rating:
|
Hi William, Thanks for the quick reply. I have attached a pdf of the program. I'm using different system clock memory bits to toggle outputs on and off at different rates. I'm using the TONR instructions to track the on time of each output. Once the first timer times out, it allows the second output to start cycling and the second timer to start accumulating time. I have tried recompiling multiple times. Again the behavior is erratic. Sometimes the cycle runs all the way to completion while other times one of the two timers "hiccups" and I have the situation shown in the screenshot from the first post. AttachmentTONR_Anomoly.pdf (124 Downloads) |
Follow us on