11/6/2014 9:25 PM | |
Posts: 1 Rating:
|
Hello! Please, help to solve the problem with communication establishment between PC and 1211C (6ES7-211-1BD30-0XB0 Firmware: V 2.0.2). I feel that i've made a stupid mistake somewhere, but cant figure out where excactly it is. So, i'm using function TRCV_С... The configuration seems to be ok: - Pic_(1) in attachment - When i set the CONT=1, the connection establishes without any problems... - Pic_(2) in attachment - But, when i set EN_R=1, i'm getting error 893A. - Pic_(3) in attachment - Thats what i have in my diagnostic buffer: (DB9 - is a block where the received data is supposed to be written) - Pic_(4) in attachment - There is an explanation given for 893A in the manuals:Parameter contains the number of a DB that is not loaded.In diag. buffer its also written that DB9 is not loaded. But in my case it is loaded! So what should i do in this case? AttachmentPictures.zip (112 Downloads) |
Last edited by: Min_Moderator at: 11/7/2014 10:42 AMMove pictures to attachment |
|
11/25/2015 3:18 PM | |
Joined: 8/21/2015 Last visit: 7/30/2020 Posts: 19 Rating:
|
Hello Huggy I have the same error 0893A showing in my RECV block like vshnukrshna.I'm attaching the pictures of the error and my program blocks.Can you please enlighten me more about the TCON parameter data type and where did I go wrong. Thank you in advance.
Attachmentconnect user properties.zip (112 Downloads) |
Last edited by: sandeep.edara at: 11/25/2015 3:19:53 PM |
|
11/25/2015 5:01 PM | |
Joined: 8/21/2015 Last visit: 7/30/2020 Posts: 19 Rating:
|
where should I change the data type ? It's fixed and I'm unable to change them.Kindly please check the figures attached .Thanks for your kind reply.
Attachmentou1.zip (98 Downloads) |
11/26/2015 9:17 AM | |
Joined: 8/21/2015 Last visit: 7/30/2020 Posts: 19 Rating:
|
I didn't use any TCON block but instead I used TCON_IP_V4 datatype in my send and receive blocks.I almost created the program just as showed in the siemens manual. https://cache.industry.siemens.com/dl/files/808/67196808/att_108115/v1/net_s7-1200_isoontcp_en.pdf Now after I changed to TCON_IP_V4 parameter i ended with 7001 in the status which indicates start execution of the job establish connection wait for connection parameter. AttachmentTconnect db.zip (86 Downloads) |
11/26/2015 10:21 AM | |
Joined: 8/21/2015 Last visit: 7/30/2020 Posts: 19 Rating:
|
yes Duris I was using iso on tcp as my connection type. |
This contribution was helpful to
1 thankful Users |
Follow us on