2/13/2014 2:52 PM | |
Posts: 1 Rating: (0) |
Hello, I have a problem reading parameters from the drive using acyle comunication using WRREC block to send request and then RDREC block to read actual values which are stored in DB. Once I activate WRREC status goes to 16#0070_0100 and then to 16#0070_0200, after that any error comes out which is 16#DF80_B000. My first question is should that status 16#0070_0200 come up?, which I believe mean "data record transfer already active", if not how to resolve that problem. I am ataching my data block in case problem is in there. Cycle comunication works fine without problems using telegram 352. Thanks in advance for any help. Attachmentdata_block.pdf (214 Downloads) |
Last edited by: jakub1992it at: 2/13/2014 2:53 PM |
|