11/7/2011 12:51 PM | |
Posts: 3093 Rating:
|
Hello Occhioreffo, yes, it will work. Schneider as well as Siemens meet the Modbus RTUspecification. Regards, Kaulquappe |
11/10/2011 9:25 PM | |
Posts: 8 Rating:
|
I think also CB1241 can talk with Altivar 312 through Modbus RTU, I prefer CB1241 instead of CM1241 because it's cheaper and easier to connect. Now my question is how to connect the RJ45 port of Altivar with 6 terminals of CB1241, I suppose: ATV312 ---------------------- CB1241 5 D0 -------------------------- TRA + TA 4 D1 -------------------------- TRB + TB 8 Common bus signal --- M Do you agree? AttachmentATV312 + CB1241.pdf (646 Downloads) |
1/22/2018 2:54 PM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating:
|
New question published by Xavi17 is split to a separate thread with the subject try to make the CM1241 RS485 connector for ATV312 . Best regards |
Follow us on