7/8/2013 5:05 PM | |
Posts: 24 Rating:
|
|
7/9/2013 7:20 AM | |
Joined: 3/21/2006 Last visit: 3/19/2025 Posts: 10239 Rating:
|
It might be a problem - S7-1200 is not mentioned in description. (Cp343-1, CP443-1 and CP243 only). But selecting CP343-1 and the way of Tomy Master it might works. (take a look at official web page toohttps://play.google.com/store/apps/details?id=de.ase.s7droidlite). Best regards, Hristo Mihalev
|
This contribution was helpful to
1 thankful Users |
7/9/2013 9:49 AM | |
Joined: 11/21/2007 Last visit: 3/16/2025 Posts: 2326 Rating:
|
Dear UMENCHO Here is an extract from Version Details of S7droid lite : ------------------------ V1.2.1: Support of IBH NetLink V1.2: The communication driver now supports S7-200/S7-1200/S7-300/S7-400 and new Logo 0BA7 Devices (S7-200 Devices only in theorie, no hardware to test!) V1.1: Added Functions: Polling S7 Datapoints - the datapoints can be polled with different intervals DNS resolution - Now you can use a DynDns Name for example S7 Address Wizzard - you can open a S7-Address Wizzard for creating the Datapoint Address ------------------------- This confirms that it should work with S7-1200 but has not been tested. Good Luck Navnag |
Last edited by: Navnag at: 7/9/2013 9:49 AMThere is no such thing as the last bug in a program |
|
7/9/2013 6:54 PM | |
Joined: 11/21/2007 Last visit: 3/16/2025 Posts: 2326 Rating:
|
Hello marco23 You can Contact the developers of S7Droid through this Website ( http://www.automation-se.de/) It is in German but you can use Google Translate. However They also have a full manual on S7Droid in English at : http://www.automation-se.de/images/howtos7droidfull_en.pdf This also gives an example of connection to S7-1200. The IP address and Port Setting is Done in the parameters of Instance DBs of T_CON and T_SEND & T_RECV blocks. Pl see example attached Hope this helps Cheers Navnag |
There is no such thing as the last bug in a program |
|
7/12/2013 11:36 AM | |
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating:
|
New question splitted to link Brand T Android / Mobile Second Generation with S-1200 1214C Best regards O_Moderator |
8/7/2013 12:38 PM | |
Joined: 9/1/2005 Last visit: 3/10/2025 Posts: 4113 Rating:
|
New question splitted to cannot communicate in any cpu using s7android lite. Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on