11/30/2021 8:37 AM | |
Joined: 3/11/2019 Last visit: 1/27/2023 Posts: 601 Rating:
|
Dear Maruthupandian, as Towome already mentioned, for a CPU-1200 a SMC is needed if the password was lost. Informations can be found here: SIMATIC S7 S7-1200 Programmable controllerRecovery from a lost passwordTransfer cardregards sancruz |
Feedback appreciated, please rate |
|
This contribution was helpful to
1 thankful Users |
11/30/2021 8:18 PM | |
Joined: 11/21/2021 Last visit: 1/22/2023 Posts: 13 Rating:
|
Dear sir, I Have no 24 MB MMC CARD.. MMC 64 kb ONLY AVAILABLE. IT'S POSSIBLE? SIR |
12/1/2021 8:56 AM | |
Joined: 7/9/2015 Last visit: 1/27/2023 Posts: 3273 Rating:
|
Hi, you need a SIMATIC Memory Card (SMC). Please check this: How can you delete the IP address and reset your S7-1200 to factory settings using the SIMATIC MC memory card?Regards, Towome |
If my post was useful, please rate me - thank you! |
|
This contribution was helpful to
1 thankful Users |
12/2/2021 2:29 AM | |
Joined: 11/21/2021 Last visit: 1/22/2023 Posts: 13 Rating:
|
Dear sir, This SIMATIC MICRO MEMORY CARD POSSIBLE FOR S7 - 1214C CPU PASSWORD RESET? PLEASE REPLY ME |
12/2/2021 5:43 AM | |
Joined: 5/12/2006 Last visit: 1/27/2023 Posts: 21197 Rating:
|
this type of card is not compatible with S7-1200 an can not be used. |
Follow us on