6/10/2016 8:38 PM | |
Posts: 13 Rating:
|
Thanks, it is a bridged adapter link, pretty sure I used the same settings as the guy in this video and he seemed to have got it to work. Although his UI is in Spanish and mine in English, I'm pretty sure I have the right settings. I did have a dynamic IP on my host(win10). I will change that to fixed on Monday(I'm assuming I was a different IP to the virtual machine) and also try with VMWare instead of virtualbox as I read in another thead that that is what Siemens suggests. Firewall was disabled on the virtual machine (win7 professional sp1, 32bit). I will try disable my firewall on the host machine next time as well. I assumed I wouldn't be able to even detect the PLC or change the IP if it was a connection issue though. Another other suggestions anyone? Really need to get this to work asap :/ |
Last edited by: Derick81 at: 6/10/2016 8:42:07 PM |
|
6/11/2016 1:58 PM | |
Posts: 13 Rating:
|
Thank you, yes it did turn up under accessible devices. I will try again on Monday with your suggestions. |
This contribution was helpful to
1 thankful Users |
Follow us on