3/26/2014 5:39 PM | |
Posts: 150 Rating:
|
Dear all, I am planning an application where I need to connect 47 TH400 temperature transmitters to a S7-1500 using Profibus-PA. I have done it before in Step7 V5.5 but it looks like the Profibus-PA functionality is not build into TIA portal. My DP/PA Link consists of: 1 x 6ES7-153-2BA02-0XB0 2 x 6ES7-157-0AC83-0XA0 I found this FAQ which explains how to add PA functionality in TIA portal. What is not explained in the FAQ though is how the FDC157 added to the configuration. I am just assuming that it may be done as in the attached screenshot. I cannot test it because I dont have my hardware yet. Can anyone verify if this is the way to do it? Regards Nik. |
This contribution was helpful to
1 thankful Users |
11/8/2016 5:33 PM | |
Joined: 4/28/2015 Last visit: 11/2/2022 Posts: 1 Rating:
|
Dear Nikzitronik, Did you find a solution ? I have the same problem as you. With best regards, Nicolas. |
Follow us on