6/9/2017 8:26 AM | |
Joined: 3/3/2014 Last visit: 5/17/2022 Posts: 4 Rating:
|
Good day! I have hardware; S7-1500 and drive ATV320. Profinet communication with Telegram 100 established but i can't see data exchange. I can't see any status drive value (ETA). I try to use only MOVE function for send commands (CMD) and speed (LFRD) and see strange : if i send and control word (CMD) - QW0 to ATV320, i see this value in status word (ETA) - IW0. Why? Please help me! This is very urgent. Thank's AttachmentATV Profinet Test V2.zip (1598 Downloads) |
This contribution was helpful to
1 thankful Users |
7/31/2017 11:17 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating:
|
New question published by AlexSen is split to a separate thread with the subject ATV 930 with profinet - Don't have data exchange. Best regards |
Follow us on