3/11/2017 10:39 AM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating:
|
Hello, The technician abroad also connects with a VPN client to the same server. This is explained in this sample here: The S615 can be replace here by a M874 (the M874 can be seen as a S615 with a wireless interface). An example with an Ios Tablet An example with a PC where you could run TIA. Advantage of having a central server is the central management of the VPN settings. |
Best regards |
|
This contribution was helpful to
2 thankful Users |
3/12/2017 10:57 AM | |
Posts: 21 Rating:
|
Thank you Best regards Kostov |
Follow us on