1/17/2014 8:03 AM | |
Joined: 3/20/2013 Last visit: 3/18/2025 Posts: 676 Rating:
|
hey autogen i am not quite sure: do you want to use the existing PROFIBUS net or are you switching everything to Industrial Ethernet? you know that there is a S7-1500 with PROFIBUS interface? (The 1516-3 PN/DP. If you want to choose this one, please check before the protocols you are using and if the S7-1500 is capable of them. ) if you start buying new network devices like an OLM, perhaps you can directly switch to the SCALANCE components. Perhaps have a look at the catalogue. But if i understood your question in the right way you want to use a IE/DP Link? Have a look at this device. |
Last edited by: Fafner at: 1/17/2014 8:08 AMBest Regards, |
|
Follow us on