11/17/2020 9:52 AM | |
Joined: 10/10/2005 Last visit: 6/15/2023 Posts: 1909 Rating:
|
Hello UTE_GAW, please consider the main and load memory of the S7-1500 CPU is higher than by the S7-1200 CPU. The S7-1500 CPU Includes the simple functionality of S7-1200 and meets special demands for performance, flexibility and networkability. Regarding to improve the performance see also the FAQ: How can you improve the performance in STEP 7 (TIA Portal) and in the S7-1200/S7-1500 CPUs? With best regards |
Follow us on