5/6/2021 10:04 PM | |
Joined: 9/27/2006 Last visit: 4/26/2025 Posts: 12346 Rating:
|
Hello analoty.v; Use a switch between the S7-1500R CPUs and the HMI/PC station, as shown in the following diagram, taken from the S7-1500R/H manual: https://support.industry.siemens.com/cs/ww/en/view/109754833/129770622731 Hope this helps, |
5/7/2021 9:46 AM | |
Joined: 8/3/2009 Last visit: 4/25/2025 Posts: 15355 Rating:
|
Hello anatoly.v do you already know this FAQ: https://support.industry.siemens.com/cs/de/en/view/109781687 Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
5/13/2021 10:11 AM | |
Joined: 11/13/2013 Last visit: 12/8/2024 Posts: 35 Rating:
|
UPD: I have solved the trouble. 1. Go to "Connections" 2. RIght click on PLC 3. "Add new connection" 4. Choose interface 5. Enable "Use the system IP ..." 6. Add Manual: https://support.industry.siemens.com/cs/document/59192925/simatic-s7-1500-et-200mp-et-200sp-et-200al-et-200pro-et-200eco-pn-communication?dti=0&dl=en&lc=de-WW |
Last edited by: anatoly.v at: 05/13/2021 10:12:41Last edited by: anatoly.v at: 05/13/2021 15:09:22 |
|
This contribution was helpful to
1 thankful Users |
Follow us on