10/30/2018 3:37 PM | |
Joined: 12/13/2016 Last visit: 8/27/2019 Posts: 22 Rating:
|
Hello, I wanted to add supervisions and visualize them usinge PLC Code View object on HMI. When i write something in GRAPH and add Supervision alarm, everything works well, code is illustrated. However when i add regular supervision, after clicking alarm called by this supervision on Alarm View and after clicking "CodeView" external button i dont see the snippet fro the code which caused/triggered supervision. I Tried to followed this tutorial: https://support.industry.siemens.com/cs/ww/en/view/109740151 I noticed that when i click on prodiag alarm (Operand/Reaction) , bool variable passed in Alarm view -> Display - > Control TAG for PLC Code view doesn't change to "1". When i click on Graph supervision which works, this variable switches to "1" im using tia v 15 and win cc advanced im attaching overview screenshot |
Last edited by: Jacplacu at: 10/30/2018 3:37:34 PMLast edited by: Jen_Moderator at: 10/31/2018 9:15:55 AMOptimized link. |
|
Follow us on