5/10/2016 11:38 AM | |
Posts: 14 Rating: (0) |
Hi, I am using an S7-1511F and WinCC Professional V13 on a windows server 2012 R2. I am trying to set up time synchronization between PLC and SCADA using NTP but i get the following error: "CPU Maintenance required: Time synchronization failure: No time synchronization with time master" Event ID: 16# 02:4054. I have activated NTP on the server according to the attached manual. The server is not a domain controller and does not have any internet connection. Could this have anything to do with the error? In the HW config i have set the IP-address for the SCADA server and an update interval of 30 s. Attachment67518641_wincc_pro_timesynch_en.pdf (537 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on