10/5/2018 9:51 AM | |
Joined: 4/28/2015 Last visit: 1/25/2023 Posts: 385 Rating:
|
Hello, for stepper motor control, you could use:
In both cases, you could use the motion control objects (Technology object) and Motion control functions of the CPU to control the stepper motor. If your stepper motor driver need 5V connection, you could add a 5V signal board (6ES7222-1AD30-0XB0) to the S7-1200 to connect to the stepper motor driver. With ET200 SP TM PULSE 2x24VET200 SP TM PULSE 2x24V, you could also control a 24V DC motor up to 4A current via technology objects and motion control functions of the CPU, instead of the stepper motor. |
Follow us on