4/29/2008 11:25 PM | |
Posts: 5822 Rating:
|
Hello, well, let me try to answer. To 1. You can do S7 Connections between the S7-300 and the S7-200 over Ethernet. There you can run S7-Functions PUT / GET on a both sided configured Connection. See: How do I configure an S7 connection for data communication between an S7-200 and an S7-300 via Ethernet? To 2. The CP 243-1 can run up to 8 S7-Connections. So you should be able to have 4 PCs on the same CP. There I see no problem. Best regards J_Bell |
4/30/2008 3:17 PM | |
Posts: 5822 Rating:
|
Hello, |
4/30/2008 4:06 PM | |
Posts: 5822 Rating:
|
Hello, well, please check this FAQ: How do I configure an S7 connection for data communication between an S7-200 and an S7-300 via Ethernet? If you want to write form the S7-300 to the S7-200 you will have to use the DB1, the DB1 is the VB area in the S7-200. Best regards J_Bell |
Follow us on